This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 connect to a 4 *8 DataWidth DDR3 device,will the performance be influenced?

Hi,TIer.

I wanna use C6678 to connect 4 *8 DataWidth DDR3 devices,as the C6678's DDR3 data port's width is 64,A 32bit width will influence the C6678's performance?If the operating frequency is the same.

We wanna use C6678 to do H.265 encode/decode,such as enode a 720P30 video into H.265 bitstream.