This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question on AM335x CAN subsystem, message receiving

Hi,

I am using the AM335x ICE v2.1 to receive CAN messages. I wish to
program different CAN message objects in the message RAM to receive
different ID messages. (NOTE This is under SYS/BIOS). I have it
successfully receiving messages but cannot seem to make it selective.
That is if I program a a slot with ID= 0x381 it receives messages with
that ID but also with 0x382...

I am using the code from dcanTxRx and the drivers and platform code for
the V2.1 AM335x ICE as I have detailed in other messages on using CAN
under SYS/BIOS. In the code for dcan_frame.c the routine

unsigned int CANRxObjectConfig(unsigned int baseAdd, can_frame* canPtr)

does this:

/* Use Acceptance mask. */
DCANUseAcceptanceMaskControl(baseAdd, DCAN_MASK_USED, DCAN_IF2_REG);

/* Configure the DCAN mask registers for acceptance filtering. */
DCANMsgObjectMskConfig(baseAdd, DCAN_IDENTIFIER_MSK(DCAN_ID_MASK,
DCAN_ID_MSK_11_BIT), DCAN_MSK_MSGDIR_DISABLE,
DCAN_MSK_EXT_ID_ENABLE, DCAN_IF2_REG);

This does not seem correct shouldn't it be DCAN_MSK_MSGDIR_ENABLE
instead of DCAN_MSK_MSGDIR_DISABLE ?

However if I do that, putting this line in instead:

DCANMsgObjectMskConfig(baseAdd, DCAN_IDENTIFIER_MSK(DCAN_ID_MASK,
DCAN_ID_MSK_11_BIT), DCAN_MSK_MSGDIR_ENABLE,
DCAN_MSK_EXT_ID_ENABLE, DCAN_IF2_REG);

with the Enable instead is has no effect I still receive messages with the wrong ID.

I have also tried:

DCANMsgObjectMskConfig(baseAdd, DCAN_IDENTIFIER_MSK(DCAN_ID_MASK,
DCAN_ID_MSK_11_BIT), DCAN_MSK_MSGDIR_ENABLE,
DCAN_MSK_EXT_ID_DISABLE, DCAN_IF2_REG);

using DCAN_MSK_EXT_ID_DISABLE instead of ENABLE.

Any suggestions of what I can do here. I am using the dcanTxRx code and
monitoring the interrupt routine void DCANIsr0(void)() for receipt of
the packet.

Thanks,

--jim schimpf