Hi,
I have a custom 8148 board, on which has KSZ9031RNX phy connected to phy address 0x3.
When I do tftp I get timeout errors,
dm8148#dhcp
phyid: 221622
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
DHCP client bound to address 192.168.1.122
dm8148#tftp 0x80009000 uImage
phyid: 221622
link up on port 0, speed 1000, full duplex
Using cpsw device
TFTP from server 192.168.1.115; our IP address is 192.168.1.122
Filename 'uImage'.
Load address: 0x80009000
Loading: T T T T T T T T #################################################################
#################################################################
#################################################################
#################################################################
#############################T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T T
CTRL-A Z for help | 115200 8N1 | NOR | Minicom 2.7 | VT102 | Offline | ttyUSB0
On the evm it works fine, is there any fix or I should something to look at ?
I have observed that after transferring the same size the timeout starts again.
Thanks & Regards,
Mike