I'm seeing what appear to be several related bugs in Grace 3.0.1.59:
1. When changing the comparator reference level using a resistor ladder , Grace does not recognize and change to the configuration file.
2. When initializing the comparator, since it does not see the reference level set to say "31/32", it assumes 32/32 and turns the resistor ladder off.
Ironically, a previous setup did have the parameter: Comparator_D.compdDividerNumerator0 used, but now even if I add it back in manually, the interface does not show the value.