Other Parts Discussed in Thread: TMS320C6416
hello,
I'm using the EMIF data pins for control a DAC board,
I have the emif clock connected to ground, pin 78 of J3.
This is a part of my code
//defino la salida de la placa# define OUTPUT 0xA0000000unsigned int *output =(unsigned int*)OUTPUT;unsigned int exit;void setup(){ /*iniciamos un vector con todo 0 menos el W/R que lo dejamos a uno posicion 25*/ exit=0;//32 bits a 0; exit = (1<<24 | exit); *output=exit;//escribimos en memoria;}void main(){ setup();it's working correctly, but I need control a ADC board, i know that the DSK board have his own's conversors, but I need the DC. I know the limitations that have the audio conversor.
I only want do the same using the HD data bus[0:31], in some documents I read that they are named AD[0:31].
Thanks