This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

McBSP configuration to provide internal clock to Audio Codec in dm365 evm.



Currently provide external clock to codec through crystal in dm365.

But need to provide clock from on chip clock source.

For that, what are the register value changes require in  McBSP.

And in which files that can be done?

Specifications:

Hardware: TI tms320dm365

Software: Linux kernel 2.6.32.17

Audio Codec: TVL320AIC3101.

Thanks.