Hi
I need to change the inter-byte timing of a SPI data packet when sending from 8148 to device. Any advice on which register I should use? Thanks.
Rgds
Dan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I need to change the inter-byte timing of a SPI data packet when sending from 8148 to device. Any advice on which register I should use? Thanks.
Rgds
Dan
Moving this to the DM814X forum.
Dan,
I have checked the DM814x McSPI module registers, and I found just one time control register:
MCSPI_CH(i)CONF[26:25] TCS
This is programmable timing control between chip select and external clock generation. For more info see DM814x TRM, sections 22.3.12 McSPI Channel (i) Configuration Register (MCSPI_CH(i)CONF) and 22.2.3.8 Chip-Select Timing Control
See also the below e2e threads:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/302472.aspx
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/93517.aspx
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/t/37920.aspx
BR
Pavel