Dear Sir,
I have a beaglebone black and ezsdk 7.00.00. I would need to rotate 90 degrees the hdmi screen for a portrait application. Wich settings do I have to adjust?
Best regards.
Julio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Julio,
The AM335X LCD controller does not support rotation.
The only way I see it is to reconfigure the frame buffer, but I don't know if the HDMI transmitter will support this.
Biser,
One more question:
Our idea is using also wl1831 module. Is beagleboard-xm compatible with WL1835MOD cape or with WL1835MOD EVK from TI?
Best regards and thanks in advance.
This is the beagleboard-xm page: http://beagleboard.org/beagleboard-xm You can find all information resources about the board there.