This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need to provide CLKOUT0 to MCLK of audio codec in dm365.

Need to provide CLKOUT0 to MCLK of audio codec TVL320AIC3101 with 24 MHz.

Specifications:

Hardware: TI tms320dm365

Software: Linux kernel 2.6.32.17

Audio Codec: TVL320AIC3101.

For that changed PINMUX4 register with enabling 21-20 bit with value '1' to enable CLKOUT0.

Also made hardware connection from processor to MCLK as per schematic.

Now to make it work what extra things need to change ?

Please suggest extra changes for kernel files,audio codec file and others if any.

Thanks.