Hello, I am trying to use the GPIO 61 and 62 on our design using the DM368 processor, but I'm not seeing the correct signal on the pin. I have configured them as outputs, and other GPIOs in bank 2 work ok. The GIO[57..64] are muxed with AEMIF EM_D[8..15], but we are using the 8-bit AEMIF interface for boot. The BOOTCFG register is 0x00000032, which means AECFG is 010, and so the GIO[57..64] should be enabled. Please tell me something I missed to enable those GPIOs, or any other suggestions?