This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Slow DSP67x.lib

I am using the DSP67x.lib with the OMAP L137. I am comparing the single precision dot-product (multiply-add) to the C language equivalent and there is not much difference.  For example, a 1000 point multiply-add should take about 1000/2 * 10 ns = 5 us and it is taking about 120 us on a 300 MHz OMAP 674x DSP. It is as if the instruction cache is not enabled. When I execute the GEL command to enable the instruction cache, I get

Enable_Instruction_Cache() cannot be evaluated.

identifier not found: CPSR

at CPSR=0x400000d3 [dskda830_dsp.gel:637]

at Enable_Instruction_Cache()

Any ideas?