In my MessageQ program, the msmcsram is as sharedregion0. When i disable the cache,the ipc_start() didn't return.
The cfg file is follow:
/* Shared Memory base address and length */
var SHAREDMEM = 0x0c300000;
var SHAREDMEMSIZE = 0x00100000;
SharedRegion0.translate = false;
SharedRegion0.setEntryMeta(0,
{ base: SHAREDMEM,
len: SHAREDMEMSIZE,
ownerProcId: 0,
cacheLineSize: 0,
cacheEnable: false,
isValid: true,
name: "MSMCSRAM_IPC",
});
when i pause the core0, it shows that
But when i enable the cache,the program can work well,the .cfg file is that:
/* Shared Memory base address and length */
var SHAREDMEM = 0x0c300000;
var SHAREDMEMSIZE = 0x00100000;
SharedRegion0.translate = false;
SharedRegion0.setEntryMeta(0,
{ base: SHAREDMEM,
len: SHAREDMEMSIZE,
ownerProcId: 0,
cacheLineSize: 128,
cacheEnable: true,
isValid: true,
name: "MSMCSRAM_IPC",
});
Does the sharedregion 0 must be cached?