This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

boundary scan mode for TMS320C6713GDPA200

hi,

now i having problem to test this device using Agilent 3070 through boundary scan test. The device is not respond as desire and it seen like the instruction register length is not right.

i've drive emu0, emu1 and rst to "0".


in order for this device to change to boundary scan mode, is the device need to boost up properly 1st? or is there any other method that miss out in datasheet?

regards,

kevin