Other Parts Discussed in Thread: 66AK2H12
hi, everyone
========================================================================
My test environmemt
Using EVM : EVMK2H
EVM A Ethernet Port 1 <---> EVM B Ethernet Port 1 : Connected Ethernet Cable
Example Project : PA_emacExample_K2H66BiosExampleProject(source modified for test)
EVM A, B : CPSW_LOOPBACK_NONE
EVM A : Transmitter (Continue SendPacket (0))
mac address : 0x00, 0x01, 0x02, 0x03, 0x04, 0x05
ip address : 192.168.1.1
port : 0x1234
EVM B : Receiver (waiting Cpsw_RxISR())
mac address : 0x10, 0x11, 0x12, 0x13, 0x14, 0x15
ip address : 192.168.1.10
port : 0x5678
*. PC is confirmed that the frame sent from the EMV A. (Using wireshark)
========================================================================
Qusetion !!
EVM B' Cpsw_RxISR is not triggered.
But,
EVM B' STATB(0x02090c00) RXGOODFRAME increses.
Frame number of Transmitter is equal to EVM B' STATB RXGOODBRAME Number.
Why Cpsw_RxISR is not triggering?
please help!
regards.