This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding QWSSocket::connectToLocalFile could not connect:: Connection refused error for dra7xx-evm

Hello,

We are working on dra7xx-evm(OMAP5777)  board. Here we are using these things:

1.  linux-3.12 kernel

2. Toolchain- gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.

3. Filesystem- arago-glsdk-multimedia-image-dra7xx-evm.

4. glsdk_6.10.00.02

5. qt 4.8.4 

Sample Qt code is working fine on this board.


We are trying to build a Qt-project  which will take library from the another Qt-library project.

We are able to build Qt-library project and also able to include this library in our Qt-project, this project is building fine.

Before running this application, we have put all the required shared library into /usr/lib folder.

But during running this application(./sample  -qws )

It is showing the following log:

Enter the start as 1

1

Changing Configuration parameters

1. Operation Mode (1->Tx 2->BITE)

2. Range (1->4M 2->8M 3->16M)

Thread executing ...

3. Active Mode (1->Normal 2->Tracker 3->Doppler)

4. Data Log (1->Enable 0->Disable)

5. Read Back (1->Enable 0->Disable)

6. Play Back (1->Enable 0->Diable)

7. Wi-Fi (1->Enable 0->Disable)

8. Battery (0-100)

9. Normal Data

10. Tracker Data

11. Exit

QWSSocket::connectToLocalFile could not connect:: Connection refused

QWSSocket::connectToLocalFile could not connect:: Connection refused

QWSSocket::connectToLocalFile could not connect:: Connection refused

QWSSocket::connectToLocalFile could not connect:: Connection refused

QWSSocket::connectToLocalFile could not connect:: Connection refused

QWSSocket::connectToLocalFile could not connect:: Connection refused

No Qt for Embedded Linux server appears to be running.

If you want to run this program as a server,

add the "-qws" command-line option.

 

Please help in this regard.

Regards

Naveen