Is TI's EVMK2H Evaluation board electrically and mechanically compatable with the TMDXEVMPCI AMC to PCIe Adapter card?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is TI's EVMK2H Evaluation board electrically and mechanically compatable with the TMDXEVMPCI AMC to PCIe Adapter card?
No. The TMDXEVMPCI is only compatible with KeyStone I EVMs.
The only other option I know is breakout cards connected with SMA cables. You can use an AMC SMA breakout card such as the AMC SMA ULTRA 9000 connected to the PCIE connector with a PCIE adapter cable. This would allow the PCIE interface of the K2H EVM to be connected to a system with a PCIE connector. Remember that you will need to include the 100MHz reference clock in your connections if your target system operates with a spread spectrum clock.
Regards, Bill