Other Parts Discussed in Thread: TMS320C6678
I am porting some code to test on a TMS320C6678 EVM board, and having trouble with the linker.
The messages I am getting are:
warning #10247-D: creating output section ".TI.tls" without a SECTIONS specification warning #10247-D: creating output section ".TI.tls_init" without a SECTIONS specification "rand.c", line 54 (approximate): warning #17003-D: relocation from function "rand" to symbol "next" overflowed; the 22-bit relocated address 0x20c797 is too large to encode in the 15-bit unsigned field (type = 'R_C6000_TPR_U15_W' (40), file = "C:\ti\ccsv5\tools\compiler\c6000_7.4.11\lib\rts6600_elf_mt.lib<rand.obj>", offset = 0x00000008, section = ".text:rand") "rand.c", line 54 (approximate): warning #17003-D: relocation from function "rand" to symbol "next" overflowed; the 22-bit relocated address 0x20c797 is too large to encode in the 15-bit unsigned field (type = 'R_C6000_TPR_U15_W' (40), file = "C:\ti\ccsv5\tools\compiler\c6000_7.4.11\lib\rts6600_elf_mt.lib<rand.obj>", offset = 0x0000002c, section = ".text:rand") "errno.c", line 86 (approximate): warning #17003-D: relocation from function "__c6xabi_errno_addr" to symbol "__errno" overflowed; the 24-bit relocated address 0x831e2c is too large to encode in the 15-bit unsigned field (type = 'R_C6000_TPR_U15_B' (38), file = "C:\ti\ccsv5\tools\compiler\c6000_7.4.11\lib\rts6600_elf_mt.lib<errno.obj>", offset = 0x0000000c, section = ".text:__c6xabi_errno_addr") warning #10015-D: output file "benchmark.out" cannot be loaded and run on a target system
I have looked at several articles, and so far tried the following:
- --mem_model:data to far
- Various changes to the .cfg file
- Checked that the issue in
doesn't apply ( I am using compiler 7.4.11, the header is already modified as expected)
I understand what relocation does, but I'm not clear how I can fix the way these library functions are relocated. I presume this should be an easy fix, but I'm stuck, what should I do?