Hi,
we are using ti-rmd5_rdk_1.0.0. there are some question in booting log.
what is mean about RED color in line. do we need the Mem map bin file for M3 FW??
if so. how to set the mem map.bin.
if not. is there any issue when we got RED color message??
log**********************************************************
SysLink version : 2.10.03.20
SysLink module created on Date:Sep 10 2014 Time:05:03:09
FIRMWARE: Memory map bin file not passed
Usage : ./firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
Syslink: _NotifyDrvUsr_eventWorker thread created, tid = 1055
Syslink: _NotifyDrvUsr_eventWorker: set real-time priority of 32
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 1 start Successful
FIRMWARE: Memory map bin file not passed
Usage : ./firmware_loader <Processor Id> <Location of Firmware> <start|stop> [Location of Mem map bin file]
FIRMWARE: Default memory configuration is used
MemCfg: DCMM (Dynamically Configurable Memory Map) Version : 2.1.1.1
Syslink: _NotifyDrvUsr_eventWorker thread created, tid = 1057
Syslink: _NotifyDrvUsr_eventWorker: set real-time priority of 32
FIRMWARE: Memory Configuration status : In Progress
FIRMWARE: 2 start Successful
VPSS_FVID2: M3 firmware version 0x1000143 is newer,driver may not work properly.
**********************************************************
Austin Huang