This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127IPNC : the implementation of mplayer

Hello:

I need to play mp3 files on the DM8127IPNC with mplayer and I followed the steps from http://processors.wiki.ti.com/index.php/Mplayer. unfortunately it doesn't work.

configuration as below:

./configure --enable-cross-compile --cc=arm-none-linux-gnueabi-gcc --host-cc=gcc --as=arm-none-linux-gnueabi-as --ar=arm-none-linux-gnueabi-ar --ranlib=arm-none-linux-gnueabi-ranlib --target=arm-linux --enable-alsa switch --prefix=/home/derec/DM8127/MPlayer/MPlayer_Out

The procedure of configuration can be done, but some error would show when make:

vo_fbdev.c: In function 'config':
vo_fbdev.c:802: warning: unused variable 'zoom'
arm-none-linux-gnueabi-gcc -I../libavcodec -I../libavformat -Wdisabled-optimization -Wno-pointer-sign -Wdeclaration-after-statement -I. -I.. -I../libavutil -Wall -Wno-switch -Wpointer-arith -Wredundant-decls -O4   -pipe -ffast-math -fomit-frame-pointer -D_REENTRANT -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64 -D_LARGEFILE64_SOURCE -DHAVE_CONFIG_H    -c -o vo_fbdev2.o vo_fbdev2.c
arm-none-linux-gnueabi-gcc -I../libavcodec -I../libavformat -Wdisabled-optimization -Wno-pointer-sign -Wdeclaration-after-statement -I. -I.. -I../libavutil -Wall -Wno-switch -Wpointer-arith -Wredundant-decls -O4   -pipe -ffast-math -fomit-frame-pointer -D_REENTRANT -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64 -D_LARGEFILE64_SOURCE -DHAVE_CONFIG_H    -c -o vo_pnm.o vo_pnm.c
arm-none-linux-gnueabi-gcc -I../libavcodec -I../libavformat -Wdisabled-optimization -Wno-pointer-sign -Wdeclaration-after-statement -I. -I.. -I../libavutil -Wall -Wno-switch -Wpointer-arith -Wredundant-decls -O4   -pipe -ffast-math -fomit-frame-pointer -D_REENTRANT -D_LARGEFILE_SOURCE -D_FILE_OFFSET_BITS=64 -D_LARGEFILE64_SOURCE -DHAVE_CONFIG_H    -c -o vo_ivtv.o vo_ivtv.c
vo_ivtv.c: In function 'ivtv_reset':
vo_ivtv.c:79: error: storage size of 'sd' isn't known
vo_ivtv.c:80: error: storage size of 'sd1' isn't known
vo_ivtv.c:84: error: 'IVTV_STOP_FL_HIDE_FRAME' undeclared (first use in this function)
vo_ivtv.c:84: error: (Each undeclared identifier is reported only once
vo_ivtv.c:84: error: for each function it appears in.)
vo_ivtv.c:87: error: 'IVTV_IOC_STOP_DECODE' undeclared (first use in this function)
vo_ivtv.c:97: error: 'IVTV_IOC_START_DECODE' undeclared (first use in this function)
vo_ivtv.c:80: warning: unused variable 'sd1'
vo_ivtv.c:79: warning: unused variable 'sd'
make[1]: *** [vo_ivtv.o] Error 1
make[1]: Leaving directory `/home/derec/DM8127/MPlayer/MPlayer-1.0rc2/libvo'
make: *** [libvo/libvo.a] Error 2

please give me some advises to fix it, thanks.

 

Derec