This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8148 _EVM

Hi,

We are planning to use TMS320DM8148CCYE1 DaVinci video processor  in our project. But the booting flash used in the EVM  MT29F2G16AADWP:D (Micron) is not available.

Can u please suggest the alternate part for this??

Thanks,

Madhura

  • Hello,

    I moved this thread to the DM814x forum.

    Madhura Shetty said:

    But the booting flash used in the EVM  MT29F2G16AADWP:D (Micron) is not available.

    Can u please suggest the alternate part for this??

    You can use any ONFI compliant flash for booting and any flash for data storing. Regarding booting from NAND flash, see DM814x TRM, chapter 4 ROM Code, section 4.7.3 NAND, Table 4-14. Supported NAND Devices

    BR
    Pavel

  • See also the below pointers:

    http://processors.wiki.ti.com/index.php/Davinci/Sitara/Integra_Nand_Boot_FAQ

    http://processors.wiki.ti.com/index.php/Determining_compatibility_between_ROM_Bootloader_%28RBL%29_and_Raw_NAND_devices

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/227978

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/233142

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/224695

    BR
    Pavel