Power domain -- Default value after reset Alaways domain _1; other domains _0 (SPRUGV4C page 17)
Clock domain -- Default value after reset C66x domain and never-gated domain _0x3; other domains _0 (SPRUGV4C page 20)
Belows are the power domain and clock domain status I got after powerup. PD_STAT and MD_STAT for MSMCRAM are also on after powerup. Is MSMCRAM considerd a C66x domain? I want to double check whether MSMCRAM is ON by defaul so that secondary boot codes can be put on it.
PD status @ powerup
PD_STATE[0] = 0x1
PD_STATE[1] = 0x0
PD_STATE[2] = 0x0
PD_STATE[3] = 0x0
PD_STATE[4] = 0x0
PD_STATE[5] = 0x0
PD_STATE[6] = 0x1
PD_STATE[7] = 0x1
PD_STATE[8] = 0x0
PD_STATE[9] = 0x0
PD_STATE[10] = 0x0
PD_STATE[11] = 0x0
PD_STATE[12] = 0x0
PD_STATE[13] = 0x1
PD_STATE[14] = 0x0
MD_STATE[0] = 0x3
MD_STATE[1] = 0x3
MD_STATE[2] = 0x3
MD_STATE[3] = 0x0
MD_STATE[4] = 0x0
MD_STATE[5] = 0x0
MD_STATE[6] = 0x0
MD_STATE[7] = 0x0
MD_STATE[8] = 0x0
MD_STATE[9] = 0x0
MD_STATE[10] = 0x0
MD_STATE[11] = 0x0
MD_STATE[12] = 0x0
MD_STATE[13] = 0x3
MD_STATE[14] = 0x3
MD_STATE[15] = 0x0
MD_STATE[16] = 0x0
MD_STATE[17] = 0x0
MD_STATE[18] = 0x0
MD_STATE[19] = 0x0
MD_STATE[20] = 0x0
MD_STATE[21] = 0x0
MD_STATE[22] = 0x0
MD_STATE[23] = 0x3
GanZ