This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM648 UART

Hello,

I am trying to implement a UART layer on the DM648 using TI sample code founder under dvsdk_1_10_00_26_DM648. When I call GIO_create():

hUart_IN  = GIO_create("/UART0",IOM_INPUT,&echoTskStatus,&chanParams,&gioAttrs);

it returns a null pointer. I stepped through the function, and the problem is at this line:

name = DEV_matchJ(name, &entry);

DEV_matchJ returns null pointer, meaning that it does not recognize "UART0".

Now I am stuck. I am not able to find the DEV_match definition, so I can debug the function.

Any help/suggestions?

Thank you.

Alin