This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Programming AM335x NAND MLO and u-boot using linux



We have an SD card and NAND on our board.  On a virgin board, (NAND not programmed) I program the SD card with a full system and boot and run from it.  For production, we boot and run from NAND.  To do this I program the NAND while running from the SD card.  Since I have linux running, I do all the programming from linux (rather than from u-boot).  This includes programming the 4 MLO partitions, u-boot, image, and rootfs.  This is easy enough to do using the MTD flash_erase and nandwrite utilities for MLO, u-boot and image, and related ubi- utilties for our ubifs rootfs.  This has all been working fine.

My question is, I do not see any examples of programming MLO from linux, but rather what I see always uses u-boot.  And some of these examples show concern for setting the ecc correctly for the MLO partitions.  Is this something I need to be concerned about?  It looks like this may have been an issue with earlier u-boot and/or linux kernels, but I believe u-boot is now using ECC8 by default and that is what we have it set for in linux.  So I think we are OK.  But I just wanted to check.

Our board is based on the ti-sdk-am335x-evm-05.06.00.00.  We have a Micron NAND IC of the same general type as is on the eval board (MT29F4G08ABBDAH4).  Our Linux is 3.2.0, and u-boot is 2012.10.

Thanks in advance for any insights.

  • Hi Rod, 

    Rod Campbell1 said:
    And some of these examples show concern for setting the ecc correctly for the MLO partitions.  Is this something I need to be concerned about?

    if you keep the selected ECC scheme in sync with Linux,you should be fine. From your post I see you've already done that, so you shouldn't have problems booting your board from NAND.


    Best Regards,

    Yordan