hi all
I test the new cpu card omap 3530 pop
The DDR RAM work OK(test from U-Boot).
The same on the EVM from mistral.
I try to program the flash and I get error .
I do the fooling step for Flashing U-Boot:
nand unlock
nand erase 0x80000 0x80000
nand ecc sw
nand write.i 0x80000000 80000 80000
and i get :NAND 256MiB 1,8V 16-bit: MTD Erase failure: -5
There is more step for programming new chip?
Regard .
Doron Sandroy
Software Team Leader
AGM tonson L.T.D
Cell : +972-52-6070406
Tel :+972-72-2500230
Fax :+972-72-2500231