Other Parts Discussed in Thread: TMS320DM6446
Hi to all,
In our custom design with TMS320DM6446 I would like to learn the functions that are DM6446EVM specific and where they are included in . For example do I have to patch all the three UBL, UBOOT and UIMAGE files if the clock rate of the DDR2 in the custom design is not 267 MHz but 333MHz with data rate 667 MT/s and same depth and width 64 x16 ?
Thanks
Ferhat