This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6455 CCS connection error.

Expert 1060 points


Hi, experts.

I've make 10 C6455 sample boards and have some trouble.

One of the 10 boards occurs the CCS jtag connection error and the others are fine.

I attached the ccs error message.

CCS pop up message

Error connecting to the target:
Error 0x80000244/-1202
Fatal Error during: Register, Initialization, OCS,
CPU continually indicated it was 'not ready'
This is considered a catastrophic event, user can either force CPU ready
and continue the debug process by choosing button 'YES', or abort current
by reset the system


I/O Port = 510

Board Name: C645x_XDS510USB
Cpu Name: cpu_0

Abort:  Close Code Composer Studio.
Retry:  Try to connect to the target again.
Cancel:  Remain disconnected from the target
Diagnostic: Run diagnostic utility.

CCS error message

 

Trouble Reading Memory Block at 0xafffffc0 on Page 0 of Length 0x340: Error 0x00000002/-1202 Error during: Memory, 
CPU continually indicated it was 'not ready' This is considered a catastrophic event,
user can either force CPU ready and continue the debug process by choosing button 'YES', or abort current by reset the system 

what causes this kind of error message?

what do i need to check?

Could you please give some debugging point?

Best Regards.

jay.