Hi, Everyone. Please Help me here,
I am getting these errors even though i used latest version from SVN(https://gstreamer.ti.com/gf/project/gstreamer_ti/scmsvn/?action=AccessInfo). i don't know what to do further. Please provide the solution for this.
THANKS IN ADVANCE.
config.status: executing configure-embedded-ffmpeg commands
Configuring included FFmpeg instance with args --prefix=/home/ajay/rootfs//opt --disable-ffserver --disable-ffplay --disable-ffmpeg --disable-ffprobe --enable-postproc --enable-gpl --enable-static --enable-pic --disable-encoder=flac --disable-decoder=cavs --disable-protocols --disable-devices --disable-network --disable-hwaccels --disable-filters --disable-doc --enable-optimizations --enable-cross-compile --target-os=linux-gnueabi --arch=arm --cross-prefix=arm-none-linux-gnueabi- --target-os=linux
Unknown C compiler arm-none-linux-gnueabi-gcc
arm-none-linux-gnueabi-gcc is unable to create an executable file.
C compiler test failed.
If you think configure made a mistake, make sure you are using the latest
version from SVN. If the latest version fails, report the problem to the
ffmpeg-user@mplayerhq.hu mailing list or IRC #ffmpeg on irc.freenode.net.
Include the log file "config.err" produced by configure as this will help
solving the problem.
config.status: error: Failed to configure embedded FFmpeg tree
make[3]: *** [ffmpeg.configure] Error 1
make[3]: Leaving directory `/home/ajay/gstreamer_ti_dm81xx/opensource_build'
make[2]: *** [.plugins] Error 2
make[2]: Leaving directory `/home/ajay/gstreamer_ti_dm81xx/opensource_build'
make[1]: *** [opensource_build] Error 2
make[1]: Leaving directory `/home/ajay/gstreamer_ti_dm81xx'
make: *** [all] Error 2
thank you
BR
Ajay Kumar KR