8168 cannot output 1080p via hdmi,
when install ti81xxhdmi.ko, error occurred:
I2C No Ack
HDMI failed to read E-EDID
what to do to remove errors?
3Q
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
8168 cannot output 1080p via hdmi,
when install ti81xxhdmi.ko, error occurred:
I2C No Ack
HDMI failed to read E-EDID
what to do to remove errors?
3Q
Hi ,
Did you tried bootlogo feature under uboot. HDMI is supported in uboot by default.
Key in 'colorbar' then you should be able to see colorbar test pattern from HDMI out.
The message of HDMI failed to read E-EDID doesnt mean there is issue on your HDMI output, it means it fails to read EDID from the monitor connected.
I will suggest you use bootlogo feature first to make sure that the hardware side is OK then we can move forward to check the software side.
BR,
Eason