Greeting!
I have to design a board with AM437x Sitara and DDR3 memory,
Then I was readign the datasheet, I found the next phrase, which I cant understand,
When not using all or part of a DDR3 interface, the proper method of handling the unused pins is to tie off the
DDR_DQS[n] pins to the VDDS_DDR supply via a 1-kΩ resistor and pulling the DDR_DQS[n] pins to ground via
a 1k-Ω resistor. (5.12.8.2.1.3.1 DDR3 Interface Schematic, document sprs851a),
Am I understand right that I have to connect unused DDR_DQS pins to VDDS_DDR pin through 1k resistors and DDR_DQSn pins to ground (GND) through 1k resistor too?
Thanks,
Ilya