Other Parts Discussed in Thread: TWL6040
Hi,
In my project i am using omap4430 & twl6040.
i am able to record voice using Sound recorder application with headset. But if i using tinycap application headset recording in playback loop is not working.
Commands i am issuing are
#DL configuration
tinymix 38 1 #DL1 PDM Switch
tinymix 50 0 #DL2 Mixer Tones
tinymix 54 1 #DL1 Mixer Tones
tinymix 78 1 #Earphone Playback Switch
tinymix 81 0 #Headset Right Playback
tinymix 82 0 #Headset Left Playback
tinymix 83 0 #Handsfree Right Playback
tinymix 84 0 #Handsfree Left Playback
tinymix 7 0 #DL1 Tones Playback Volume
tinymix 35 118 #DL1 Gain
#UL configuration
tinymix 4 2 #AMIC Equalizer
tinymix 60 11 #MUX_UL11
tinymix 61 11 #MUX_UL10
tinymix 86 0 #Analog Left Capture Route
tinymix 56 1 #DL1 Mixer Capture
tinymix 9 115 #DL1 Capture Playback Volume
tinycap /data/a.wav -d 1 -c 2 -e 3 -r 48000 -b 32 -t $1
using above sequence i am observing with below cmd
adb shell omapconf show abe atc
ATC for McPDM DL is running (Transfer form DMEM to HW IP):
ATC pointer are moving (w:5 r:5)
Base:0x40183800, iter: 24, FIFO size:120
ATC for McPDM UL is running (Transfer form HW IP to DMEM):
!!! HW IP pointer not moving
!!! ABE pointer not moving
Base:0x40183a00, iter: 4, FIFO size:120
ATC for CBPr4 is running (Transfer form DMEM to HW IP):
ATC pointer are moving (w:5 r:5)
Base:0x40182400, iter: 1, FIFO size:120
ATC for CBPr5 is running (Transfer form HW IP to DMEM):
ATC pointer are moving (w:5 r:5)
Base:0x40182c00, iter: 1, FIFO size:120
Request you to please help me to resolve my issue.
Thanks,
Gaurav