Other Parts Discussed in Thread: OMAPL138, OMAP-L138
This is my first attempt at EDMA for the DSP core of the L138. It is programmed to receive McASP serial and write it to a pair of ping-pong buffers. The McASP code has been tested using CPU polling.
I have programmed the two PaRAM for ping and pong as well as PaRAM 0 (for McASP RX). The EDMA interrupt for McASP occurs as it should. I observe the addresses changing in the TC0 DFDSTBREF register, indicating that it is switching between ping and pong for the destination. However, the ping pong buffers never fill and I have a TC ERRSTAT value of 0x1 and a TC ERRDET value of 0x9 indicating "Write addressing error".
The channel destination address in the PaRAM is a (uint32_t) value thusly:
uint32_t ping_buf[BUFSIZE], pong_buf[BUFSIZE];
...
paramSet.destAddr = (uint32_t)ping_buf;
...
The source address is the McASP receive buffer DMA port address, RBUF (0x01D02000). What can I observe to see why it is not writing data to the destination?