This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSPC 8681 performance question

I'm trying to run the MPEG2 to H.264 transcode demo available in video MCSDK 2.1. But, I'm not getting fps of more than ~16.

The input is a 8Mbps 1080p MPEG2 Main profile 24 fps & I'm encoding it to 1080p H.264 24 fps 8 Mbps CAVLC High@L4.0. We're running the card in 1.25 Ghz mode. We get around ~13 fps in 1 Ghz mode. The encoder is configured to use cores 8-15 & decoder is running on core 0 as per the configuration file in the demo.

Could you please help me understand if this is a system limitation or a demo limitation or if there's something that I am not doing right?

Thanks!