Other Parts Discussed in Thread: OMAPL138, TMS320C6748
I'm having issue connecting to Client demo for NDK with either telnet or Http.
I am able to ping the board.
the CCS console outputs the following when the code is run:
[C674X_0] Using default MAC address
Using MAC Address: 00-08-ee-03-14-99
00000.000 MAC Address = 00-08-ee-03-14-99
00000.000 EMAC should be up and running
00000.000 EMAC has been started successfully
00000.000 Registeration of the EMAC Successful
Network Added: If-1:192.168.1.80
Service Status: Telnet : Enabled : : 000
Service Status: HTTP : Enabled : : 000
Link Status: 100Mb/s Full Duplex on PHY 0
I am using:
NDK 2.24.1.18
nsp 1.10.2.09
SYS/BIOS 6.41.0.26
TIRTOS for c6000 2.0.1.23
XDCtools version 3.30.3.47_core
Any Ideas as to why it is not connecting?