This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

example program to use the FFTC in c6670



hi all

i've installed the BIOS MCSDK package . now i dont find examples to use the co processor for fft/ifft. there is only an example program for generating fft of a sequence using dsp library. if they are available, please specify the directory in which the examples are present. i am trying to open these with cc studio v5.5 only. just installing MCSDK is sufficient or do i need to do something else?

regards
phani tej