This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IP address setting by Qt



Hi All,

I have the following code written in Qt to set the ethernet intefaces parameters :

void NetworkItfManager::setItfParams( QString& itfName, EthItf_t & params )
{
    QString cmd = QString("ifconfig %1 %2 netmask %3 broadcast %4").arg(itfName, params.m_ip, params.m_netmask, params.m_broadcast);
    QProcess bashCmd;

    bashCmd.start( cmd );

    while (bashCmd.waitForFinished()) ;
}

And I believe it works fine under Ubuntu when running the application with admin rights. But with Sitara SDK 5.0 I see it doesn't work. What is the right way to modify it? How should I set the permissions?

BR,

Dmitry