This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using EMAC0 with C6678 EVM



Hello. We are trying to use the GbE port in the backplane (EMAC0) for a test to connect the TMDSEVM6678 rev.3B  to the network via MicroTCA. We tried to modify the simplest example TCP/IP Stack 'Hello World!' that comes with mcsdk_2_01_02_06.

We've found a file with some files to be replaced in pdk_C6678_1_1_2_6, (http://processors.wiki.ti.com/images/1/11/EVM_EMAC0_en.zip) but it doesn't seem to work. We suppose they were made for an older version of pdk, because with those files we can't compile platform_lib anymore. 

Which is the simplest way to do this? We have no problem with EMAC1 on the front panel.

Thanks in advance.