This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-RTOS NDK DHCP IPADDR

Hi    all       

      TI-RTOS: v2.01.00.36

       NDK: v2.23.01.01

      CCS: v6.0.1.0040

      SYS/BIOS    6.4..02.27  GA  Release  Note

      When the program is running, I want to change the IP address at any time, I will only be able to achieve this functionality through DHCP module ?

      Will I be able to operate NDK in which modules to implement this function which during the running program can be modified at any IP address ?

       Thanks

        Lewis