This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bt.656 Camera connect to DM3730 do not work

Other Parts Discussed in Thread: DM3730

Hi,

I have a digital camera could outputs YUV422 BT.656 format video.This camera only supplys DATA[0:7] and PCLK singals,without HS and VS.

The camera was connected to DM3730 camera interface cam_d[0:7] and cam_pclk, and the cam_vs and cam_hs pin was connected to the ground to draw low.

I modified the tvp514x Linux device driver to work as my camera driver,and add codes in board-omap3evm-camera.c as follows,

static struct isp_interface_config camera_if_config = {

.ccdc_par_ser = ISP_PARLL_YUV_BT,
.dataline_shift = 0x0,
.hsvs_syncdetect = ISPCTRL_SYNC_DETECT_VSRISE,
.strobe = 0x0,
.prestrobe = 0x0,
.shutter = 0x0,
.wait_hs_vs = 2,
.u.par.par_bridge = 0x0,
.u.par.par_clk_pol = 0x0,
};

static struct v4l2_ifparm ifparm = {

.if_type = V4L2_IF_TYPE_BT656,
.u = {
.bt656 = {
.frame_start_on_rising_vs = 1,
.bt_sync_correct = 0,
.swap = 0,
.latch_clk_inv = 0,
.nobt_hs_inv = 0, /* active high */
.nobt_vs_inv = 0, /* active high */
.mode = V4L2_IF_TYPE_BT656_MODE_BT_8BIT,
.clock_min = TVP514X_XCLK_BT656,
.clock_max = TVP514X_XCLK_BT656,
},
},
};

Compiling the linux kernel without any error,camera could be found by linux system.

But when running the saMmapLoop demo,application stop at the VIDIOC_DQBUF.

Then,Something strange happened.

Application went on running and image couled be captured successfully,when a oscilloscope's TEST leads touch the DM3730 cam_vs pin.

It is possible that a rising edge was created when oscilloscope's TEST leads touch the DM3730 cam_vs ,then, camera interrupt was  triggerred and image could be captured.

My question is that "Wether or not the cam_vs pin with sync singal is needed to trigger camera interrupt, although when DM3730 camera interface work in BT656 mode".