I am working on an AM335x based board. Somehow, the INIT logging after INIT is launched such as
INIT: Entering runlevel 5
is missing from the console. I can't find how to turn it back on. Your help are greatly appreciated.
Regards,
Jing
PS: My current console log is shown below:
============================================================
U-Boot SPL 2013.01.01-svn73 (Dec 16 2014 - 10:18:49)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
OMAP SD/MMC: 0
mmc_send_cmd : timeout: No status update
Card did not respond to voltage select!
spl: mmc init failed: err - -17
OMAP SD/MMC: 0
mmc_send_cmd : timeout: No status update
reading u-boot.img
reading u-boot.img
U-Boot 2013.01.01-svn73 (Dec 16 2014 - 11:25:45)
I2C: ready
DRAM: 512 MiB
WARNING: Caches not enabled
NAND: No NAND device found!!!
0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
SF: Detected W25Q32 with page size 4 KiB, total 4 MiB
*** Warning - bad CRC, using default environment
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO
Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Net: <ethaddr> not set. Validating first E-fuse MAC
<ethaddr1> not set. Validating first E-fuse MAC
cpsw, usb_ether
get MAC Address from spiflash
SF: Detected W25Q32 with page size 4 KiB, total 4 MiB
booting from MMC1 & no insert SD
Hit any key to stop autoboot: 0
mmc_send_cmd : timeout: No status update
mmc1(part 0) is current device
mmc_send_cmd : timeout: No status update
SD/MMC found on device 1
reading uEnv.txt
** Unable to read file uEnv.txt **
reading uImage
3200704 bytes read in 342 ms (8.9 MiB/s)
Booting from mmc ...
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-3.2.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3200640 Bytes = 3.1 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
XIP Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.2.0 (root@ubuntu) (gcc version 4.7.3 20130226 (pr
erelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03)
) #1 Tue Dec 16 09:13:59 CST 2014
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
n cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pag
es: 130048
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 r
o rootfstype=ext3 rootwait ip=none mac_addr=00:00:08:C8:65:20,00:00:80:96:00:00
verbose
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 512MB = 512MB total
[ 0.000000] Memory: 513144k/513144k available, 11144k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff000000 ( 488 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc059d000 (5716 kB)
[ 0.000000] .init : 0xc059d000 - 0xc05d7000 ( 232 kB)
[ 0.000000] .data : 0xc05d8000 - 0xc0640ca8 ( 420 kB)
[ 0.000000] .bss : 0xc0640ccc - 0xc0672a2c ( 200 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrup
ts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER1 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 17895
6ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000181] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.059032] pid_max: default: 32768 minimum: 301
[ 0.059156] Security Framework initialized
[ 0.059247] Mount-cache hash table entries: 512
[ 0.059607] CPU: Testing write buffer coherency: ok
[ 0.079942] omap_hwmod: gfx: failed to hardreset
[ 0.096230] omap_hwmod: pruss: failed to hardreset
[ 0.097284] print_constraints: dummy:
[ 0.097635] NET: Registered protocol family 16
[ 0.099723] OMAP GPIO hardware version 0.1
[ 0.102275] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.104018] omap_i2c.1: alias fck already exists
[ 0.104851] omap2_mcspi.1: alias fck already exists
[ 0.105749] edma.0: alias fck already exists
[ 0.105771] edma.0: alias fck already exists
[ 0.105788] edma.0: alias fck already exists
[ 0.132513] bio: create slab <bio-0> at 0
[ 0.134780] SCSI subsystem initialized
[ 0.136077] usbcore: registered new interface driver usbfs
[ 0.136375] usbcore: registered new interface driver hub
[ 0.136570] usbcore: registered new device driver usb
[ 0.136855] registerd cppi-dma Intr @ IRQ 17
[ 0.136868] Cppi41 Init Done Qmgr-base(e087a000) dma-base(e0878000)
[ 0.136878] Cppi41 Init Done
[ 0.136902] musb-ti81xx musb-ti81xx: musb0, board_mode=0x13, plat_mode=0x3
[ 0.137176] musb-ti81xx musb-ti81xx: musb1, board_mode=0x13, plat_mode=0x1
[ 0.138269] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
[ 0.141403] print_constraints: VRTC:
[ 0.142867] print_constraints: VIO: at 1500 mV
[ 0.145205] print_constraints: VDD1: 600 <--> 1500 mV at 1262 mV normal
[ 0.147533] print_constraints: VDD2: 600 <--> 1500 mV at 1137 mV normal
[ 0.148539] print_constraints: VDD3: 5000 mV
[ 0.149966] print_constraints: VDIG1: at 1800 mV
[ 0.151416] print_constraints: VDIG2: at 1800 mV
[ 0.152856] print_constraints: VPLL: at 1800 mV
[ 0.154294] print_constraints: VDAC: at 1800 mV
[ 0.155730] print_constraints: VAUX1: at 1800 mV
[ 0.157173] print_constraints: VAUX2: at 3300 mV
[ 0.158606] print_constraints: VAUX33: at 3300 mV
[ 0.160043] print_constraints: VMMC: at 3300 mV
[ 0.160855] tps65910 1-002d: No interrupt support, no core IRQ
[ 0.162298] pca953x 1-0073: interrupt support not compiled in
[ 0.169329] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.170459] Switching to clocksource gp timer
[ 0.185541] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.185710] musb-hdrc musb-hdrc.0: dma type: dma-cppi41
[ 0.186015] MUSB0 controller's USBSS revision = 4ea20800
[ 0.186047] musb0: Enabled SW babble control
[ 0.186915] musb-hdrc musb-hdrc.0: USB OTG mode controller at e083c000 using
DMA, IRQ 18
[ 0.187065] musb-hdrc musb-hdrc.1: dma type: dma-cppi41
[ 0.187371] MUSB1 controller's USBSS revision = 4ea20800
[ 0.187398] musb1: Enabled SW babble control
[ 0.187801] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 0.187885] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
r 1
[ 0.188004] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.188018] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[ 0.188031] usb usb1: Product: MUSB HDRC host driver
[ 0.188042] usb usb1: Manufacturer: Linux 3.2.0 musb-hcd
[ 0.188052] usb usb1: SerialNumber: musb-hdrc.1
[ 0.188807] hub 1-0:1.0: USB hub found
[ 0.188837] hub 1-0:1.0: 1 port detected
[ 0.189347] musb-hdrc musb-hdrc.1: USB Host mode controller at e083e800 using
DMA, IRQ 19
[ 0.189743] NET: Registered protocol family 2
[ 0.189920] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.190206] TCP established hash table entries: 16384 (order: 5, 131072 bytes
)
[ 0.190569] TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.190742] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.190755] TCP reno registered
[ 0.190768] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.190790] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.190993] NET: Registered protocol family 1
[ 0.191227] RPC: Registered named UNIX socket transport module.
[ 0.191240] RPC: Registered udp transport module.
[ 0.191249] RPC: Registered tcp transport module.
[ 0.191258] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.191494] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.209680] VFS: Disk quotas dquot_6.5.2
[ 0.209750] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.210249] msgmni has been set to 1002
[ 0.213341] alg: No test for stdrng (krng)
[ 0.213979] io scheduler noop registered
[ 0.213993] io scheduler deadline registered
[ 0.214055] io scheduler cfq registered (default)
[ 0.215829] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.876386] console [ttyO0] enabled
[ 0.880678] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.888498] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.896324] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.904132] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.911897] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.920104] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
[ 0.936353] brd: module loaded
[ 0.944297] loop: module loaded
[ 0.947742] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.954227] i2c-core: driver [tsl2550] using legacy resume method
[ 0.960653] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.967915] Board name: A33515BB
[ 0.971290] Board version: 1.5A
[ 0.974561] SKU: SKU#01
[ 0.977107] The board is general purpose EVM with DDR3 in profile 0
[ 0.984154] da8xx_lcdc.0: alias fck already exists
[ 0.989693] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[ 1.012933] Console: switching to colour frame buffer device 100x30
[ 1.028337] omap_hsmmc.0: alias fck already exists
[ 1.033858] omap_hsmmc.1: alias fck already exists
[ 1.039962] d_can.1: alias fck already exists
[ 1.049051] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.056001] m25p80 spi1.0: w25q32 (4096 Kbytes)
[ 1.060956] Creating 1 MTD partitions on "spi_flash":
[ 1.066235] 0x000000000000-0x000000400000 : "SPL"
[ 1.072873] omap2-nand driver initializing
[ 1.077314] OneNAND driver initializing
[ 1.082262] CAN device driver interface
[ 1.086264] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.092733] d_can d_can.1: device registered (irq=55, irq_obj=56)
[ 1.140519] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.147004] davinci_mdio davinci_mdio.0: detected phy mask ffffff76
[ 1.155312] davinci_mdio.0: probed
[ 1.158867] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver RTL8211E
Gigabit Ethernet
[ 1.167879] davinci_mdio davinci_mdio.0: phy[3]: device 0:03, driver RTL8211E
Gigabit Ethernet
[ 1.176873] davinci_mdio davinci_mdio.0: phy[7]: device 0:07, driver RTL8211E
Gigabit Ethernet
[ 1.186179] usbcore: registered new interface driver zd1201
[ 1.192189] usbcore: registered new interface driver cdc_ether
[ 1.198418] usbcore: registered new interface driver cdc_eem
[ 1.204533] usbcore: registered new interface driver dm9601
[ 1.210383] cdc_ncm: 04-Aug-2011
[ 1.213924] usbcore: registered new interface driver cdc_ncm
[ 1.219831] Initializing USB Mass Storage driver...
[ 1.225147] usbcore: registered new interface driver usb-storage
[ 1.231428] USB Mass Storage support registered.
[ 1.236665] mousedev: PS/2 mouse device common for all mice
[ 1.247316] rtc-s35390a 1-0030: rtc core: registered rtc-s35390a as rtc0
[ 1.254507] i2c /dev entries driver
[ 1.258519] Linux video capture interface: v2.00
[ 1.263675] usbcore: registered new interface driver uvcvideo
[ 1.269666] USB Video Class driver (1.1.1)
[ 1.311365] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.322528] cpuidle: using governor ladder
[ 1.327428] cpuidle: using governor menu
[ 1.335471] omap4_aes_mod_init: loading AM33X AES driver
[ 1.341221] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
[ 1.347785] omap4_aes_probe: probe() done
[ 1.352522] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
[ 1.358703] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
[ 1.371204] omap4_sham_probe: probe() done
[ 1.381748] usbcore: registered new interface driver usbhid
[ 1.387650] usbhid: USB HID core driver
[ 1.393809] usbcore: registered new interface driver snd-usb-audio
[ 1.402138] ALSA device list:
[ 1.405279] No soundcards found.
[ 1.408857] oprofile: hardware counters not available
[ 1.414205] oprofile: using timer interrupt.
[ 1.418717] pktgen: Packet Generator for packet performance testing. Version:
2.74
[ 1.427056] nf_conntrack version 0.5.0 (8017 buckets, 32068 max)
[ 1.433967] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 1.439691] TCP cubic registered
[ 1.443129] NET: Registered protocol family 17
[ 1.447820] can: controller area network core (rev 20090105 abi 8)
[ 1.454427] NET: Registered protocol family 29
[ 1.459128] can: raw protocol (rev 20090105)
[ 1.463636] can: broadcast manager protocol (rev 20090105 t)
[ 1.469634] Registering the dns_resolver key type
[ 1.474672] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
rev 3
[ 1.482764] ThumbEE CPU extension supported.
[ 1.487324] mux: Failed to setup hwmod io irq -22
[ 1.493013] Power Management for AM33XX family
[ 1.497890] Trying to load am335x-pm-firmware.bin (60 secs timeout)
[ 1.504650] Copied the M3 firmware to UMEM
[ 1.509039] Cortex M3 Firmware Version = 0x181
[ 1.519248] clock: disabling unused clocks to save power
[ 1.546067] Detected MACID=0:0:8:c8:65:20
[ 1.551593] cpsw: Detected MACID = 00:00:80:96:00:00
[ 1.558923] rtc-s35390a 1-0030: setting system clock to 2013-11-03 07:16:52 U
TC (1383463012)
[ 1.568400] Waiting for root device /dev/mmcblk0p2...
[ 1.584533] mmc1: unrecognised EXT_CSD revision 7
[ 1.589484] force to use eMMC 5.0! ...
[ 1.595480] mmc1: new high speed MMC card at address 0001
[ 1.601915] mmcblk0: mmc1:0001 4FEACB 3.64 GiB
[ 1.606809] mmcblk0boot0: mmc1:0001 4FEACB partition 1 4.00 MiB
[ 1.613203] mmcblk0boot1: mmc1:0001 4FEACB partition 2 4.00 MiB
[ 1.620903] mmcblk0: p1 p2 p3 p4
[ 1.627166] mmcblk0boot1: unknown partition table
[ 1.633844] mmcblk0boot0: unknown partition table
[ 1.683035] kjournald starting. Commit interval 5 seconds
[ 1.688857] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 1.696180] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[ 1.703743] Freeing init memory: 232K
[ 5.520218] kjournald starting. Commit interval 5 seconds
[ 5.545930] EXT3-fs (mmcblk0p4): using internal journal
[ 5.551532] EXT3-fs (mmcblk0p4): mounted filesystem with ordered data mode
[ 5.715699] kjournald starting. Commit interval 5 seconds
[ 5.722738] EXT3-fs (mmcblk0p3): using internal journal
[ 5.728260] EXT3-fs (mmcblk0p3): mounted filesystem with ordered data mode
[ 5.953284] EXT3-fs (mmcblk0p2): using internal journal
[ 6.992770] Disabling lock debugging due to kernel taint
[ 7.487466] gadget: Mass Storage Function, version: 2009/09/11
[ 7.493786] gadget: Number of LUNs=2
[ 7.497660] lun0: LUN: removable file: /dev/mmcblk0p1
[ 7.503085] lun1: LUN: removable file: /dev/mmcblk0p3
[ 7.508525] gadget: Mass Storage Gadget, version: 2009/09/11
[ 7.514594] gadget: userspace failed to provide iSerialNumber
[ 7.520773] gadget: g_mass_storage ready
[ 7.525015] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 7.530685] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus numbe
r 2
[ 7.538589] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 7.545760] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[ 7.553378] usb usb2: Product: MUSB HDRC host driver
[ 7.558604] usb usb2: Manufacturer: Linux 3.2.0 musb-hcd
[ 7.564204] usb usb2: SerialNumber: musb-hdrc.0
[ 7.569601] hub 2-0:1.0: USB hub found
[ 7.573599] hub 2-0:1.0: 1 port detected
[ 8.229096] net eth0: CPSW phy found : id is : 0x1cc915
[ 8.272777] net eth1: CPSW phy found : id is : 0x1cc915
[ 8.587711] net eth0: CPSW phy found : id is : 0x1cc915
[ 8.663681] net eth0: CPSW phy found : id is : 0x1cc915
[ 9.399340] net eth1: CPSW phy found : id is : 0x1cc915
Lite-On PSS Site Monitoring Controller, All rights reserved @ 2014-2015
Today is Sun Nov 3 2013 07:17:00 @ LiteOn-SMC