This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8147 I2S master clock for McASP1

I am looking into adding the external digital audio to the DM8147 so the audio stream will be embedded into the HDMI output.

If I use the McASP1, are the following connections correct?

DM8147:                              Notes:

AUD_CLKIN0      (L5)        Master audio clock

MCA1_ACLKR    (M1)      Serial audio clock

MCA1_AXR0      (V4)       Serial data

MCA1_AXR1      (T6)        Serial data

MCA1_AXR2      (R3)        Serial data

MCA1_AXR3      (N5)       Serial data

MCA1_AFSR       (M2)      Frame Sync (or Left Right channel clock)

The one in question is Master Audio clock.

Thanks,

Tai