hi ,
Am trying to test IPC - by running two different .out in two different cores :
When i group the cores and run the code : CORE0 is getting exited immediately and the error message is "No source available for "0x800730b8" " .
Core1 is waiting for IPC attach to complete.
When i run alone code is running in core0.
Can anyone help me out how to debug this issue?
MCSDK version : 2.2.1.03
IPC : ipc_1_25_03_15
CCS : V5.5
Compiler : c6000_7.4.4