Hi,
I have problems with NDK IPv6, when I connect and disconnect several times to IPv6 socket int TCP port. At one point, the TI-RTOS breaks down and shows the error:
mmBulkAlloc(): could not allocate memory.
00292.581 out of memory: handle=0x0, size=536932020
00292.581 SB6New: Buffer OOM
I've been searching in the code the root of the problem. I found that every time a client connects to IPv6 socket(TCP), a TX and RX buffer are allocated. sock6.c:
/* Allocate Rx socket buffer */
if( Type == SOCK_STREAM )
{
if( !ps->RxBufSize )
ps->RxBufSize = SOCK_TCPRXBUF;
ps->hSBRx = (HANDLE)SB6New( ps->RxBufSize, SOCK_BUFMINRX, SB_MODE_LINEAR );
}
...
/* Allocate memory for the transmit buffer. */
ps->hSBTx = (HANDLE)SB6New( ps->TxBufSize, SOCK_BUFMINTX, SB_MODE_LINEAR );
But when the client disconnects the buffer is not released:
fdClose(socket6) [my app call] -> Sock6Close() [is not always called] -> Sock6IntAbort() [is never called] -> SB6Free()
/* Free the Rx and Tx Buffers */
if( ps->hSBRx )
SB6Free( ps->hSBRx );
if( ps->hSBTx )
SB6Free( ps->hSBTx );
As the memory is not freed, the system always breaks.
I'm using an EK-TM4C1294XL, tirtos_tivac_2_01_00_03, ndk_2_23_01_01, bios_6_40_03_39, TI v5.1.6 compiler and CCSv6.
Thanks,
Vini