All,
I've read lots of forum discussion on how to attach and configure an external SDRAM to TivaC129 but now Im' really stucked.
I'll try to summarize the fundamental steps I've understood :
1) set the cmd file with a new entry like:
SDRAM (RWX) : origin = EXRAM_BASE, length = EXRAM_SIZE
2) set the section you want to map over SDRAM:
Program.sectMap[".heapSection"] = "SDRAM";
var heapMem0Params = new HeapMem.Params();
heapMem0Params.instance.name = "heapMem0";
heapMem0Params.sectionName = ".heapSection";
heapMem0Params.size = 1024;
Program.global.heapMem0 = HeapMem.create(heapMem0Params); 
Memory.defaultHeapInstance = Program.global.heapMem0;
BIOS.heapSection = ".heapSection";
3) add a reset entry in order to initialize the SDRAM
var Memory = xdc.useModule('xdc.runtime.Memory');
Startup.resetFxn = "&Board_ResetFunc";
where Board_ResetFunc:
EPIModeSet(EPI0_BASE, EPI_MODE_SDRAM);
EPIConfigSDRAMSet(EPI0_BASE, (EPI_SDRAM_CORE_FREQ_50_100 | EPI_SDRAM_FULL_POWER | EPI_SDRAM_SIZE_64MBIT), 1024);
EPIAddressMapSet(EPI0_BASE, EPI_ADDR_CODE_SIZE_16MB | EPI_ADDR_RAM_BASE_6 );
EPIDividerSet(EPI0_BASE, 0);
while(HWREG(EPI0_BASE + EPI_O_STAT) & EPI_STAT_INITSEQ) {}
The compile process is ok, and also the loading process but when I start the debugger I don't reach the main function and if I stop the debugger the PC points to and address like 0x1a00 where no code symbol are present.
Doing a step by step debug process, the Board_ResetFunc is called correctly but after that the program stuck.
Could someone help me to understand if I'm missing something ?
Thanks in advance
Marco Crivellari