Other Parts Discussed in Thread: TVP5150, TVP5150AM1
Hi,
I am using the DM8168 processor with Silicon revision 2.1. The EZSDK version is 5_05_02_00 and my Linux version linux-2.6.37-psp04.04.00.01.
I am using TWO instances of capture devices. The first one is TVP5150 and the second one is CMOS camera (OV772x).
While registering the TVP device, it registering properly without any issue and below is the debug messages and commands:
root@dm816x-evm:~# insmod /lib/modules/2.6.37/kernel/drivers/media/video/tvp5150
.ko
root@dm816x-evm:~# modprobe ti81xxvin
tvp80 81 am1 detected.
tvp82 83 detected.
tvp5150 2-005d: chip found @ 0xba (OMAP I2C adapter)
ti81xxvin ti81xxvin: registered sub device tvp5150
ti81xxvin ti81xxvin: TI81xx HDVPSS Capture driver initialized
root@dm816x-evm:~#
When I am registering the CMOS camera its showing some error below:
root@dm816x-evm:~# modprobe ti81xxvin
ti81xxvin ti81xxvin: Error registering v4l2 subdevice
root@dm816x-evm:~#
Why it is taking only the first device and not able to register the second?.
Is there any patches or changes needs to be done in the ti8xxvin driver. If so, please provide the same to solve this issue.
Thanks in advance.
Regards,
Salih