HI
I am running the (my) program in TMS320C6670l processor in CCS 5.5 version.
MCSDK _2_00_06_18,
SYS/BIOS_6_33_02_31
Xdc tools_3_23_01_43.
A single Task is created and terminated the task using exit(0).
When i compiling (after exit the task)only. its show Exception error.
How to rectify this problem.
Error Like this:
A0=0x1 A1=0x0
A2=0x4 A3=0x0
A4=0x0 A5=0x8a4797d4
A6=0x4 A7=0x2ea
A8=0x0 A9=0x8a4797d0
A10=0x861790 A11=0x0
A12=0x0 A13=0x0
A14=0x0 A15=0x0
A16=0x10103a7 A17=0x0
A18=0x861578 A19=0x30
A20=0x0 A21=0x0
A22=0xef869dc2 A23=0x442100a2
A24=0x20040 A25=0x8000d21a
A26=0x32b792e7 A27=0x0
A28=0x0 A29=0x0
A30=0x0 A31=0x2
B0=0x1 B1=0x1
B2=0x8a4797d0 B3=0x84044564
B4=0xe B5=0x858c08
B6=0x9 B7=0x10
B8=0x24cfd516 B9=0x36
B10=0x0 B11=0x0
B12=0x0 B13=0x0
B14=0x84100f80 B15=0x8615c0
B16=0x40000000 B17=0x1f
B18=0x8a423580 B19=0x8a423580
B20=0x8a423580 B21=0x8a423580
B22=0xf B23=0x0
B24=0x50624011 B25=0xf14bbd55
B26=0x4088c803 B27=0x1014364
B28=0x0 B29=0x1
B30=0x42 B31=0x4b
NTSR=0x1020c
ITSR=0xe
IRP=0x8b74f0
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0xc
EFR=0x2 NRP=0xc
Internal exception: IERR=0x1
Instruction fetch exception
{module#23}: line 248: E_exceptionMin: pc = 0x0000000c, sp = 0x008615c0.
To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'
xdc.runtime.Error.raise: terminating execution.
Thanks and regards
sridharan.