Hi All!
We have EVMK2H board with running out-of-box Linux kernel 3.8.4
With using Packet Generator feature in linux kernel I have found
that network perfomance on send/receive packets is only about 35 megabytes/sec.
So my questions are -
* Is that normal receive speed for this board?
* How can we increase it? We need to achieve as maximum as possible receive speed on single network interface.
* Do we need to use extra instances (such as netcp library or packet accelerator) to do that?