This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 IPNC RDK DDR Frequency

Hello,

We have DM365 evm and we are using IPNC_RDK_DM36x_V5.1.0. 

Right now ddr frequency is  "DDR Hz = 243000000" I want to increase it.

Please let me know where I have to make change for the same??

  • Hi,
    Pls look into the pre_build binaries and check the ubl files there.
    For different frequencies, you can use different ubl file.

    But first please check the part number of the DM365 on your EVM can run at the frequency you want first.

    BR,
    Eason
  • Vaibhav,

    You can configure the all PLL & hence the all the pheripheral and system clocks bu modifying UBL source. Also you can use the various configurations already available in UBL directory. If you build UBL, it generates different binaries with different configurations & name are also updated accordingly. Please have a look @ your UBL directory.