Other Parts Discussed in Thread: TMS320C6678
Dear All,
We have made a customized Board using TMS320C6678 with 4GBit DDR3 Micron(MT41K256M16). 2GB capacity Total of 5chip(4Chip For 2GB capacity 1Chip for ECC).
The Parameters Of the DDR3 Chip is Given Bellow:
Therefor the Page size is 2KB.
In KeyStone Architecture DDR3 Memory Controller(SPRUGV8D), 4.3 SDRAM Configuration Register(SDCFG), BIT 0-2 Defines the Page Size.
Questions:
1. We have Configured the SDCFG Register to 2KB as per the DDR3 Datasheet. We can able the perform Read, write in DDR3 Correctly. But if we try to Load a program Through CCS we Can't?
2. We have Configured the SDCFG Register to 1KB as per the Column address. We can able the perform Read, write in DDR3 Correctly. But when we try to access the FULL 2GB there are certain data mismatch is occuring.
Any Suggestion to solve the above Issue.