This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can the dm8168 hdvpss capture any resolution ?

Dear experts

In my dm8168 system, FPGA is connected with the Video port of dm8168 and the system is needed to support some innormal resolution, for example, 720x400\1920x540 which are outside the list of the resolution supported defined in the fvid2.h. I wondor if the VIP could capture such video standards?( if the timing of the signals such as hsync,vsync,de, pClk meet the capture needs).

BR.