This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM816x USB CDC_ACM device not created in /dev

Hello all,


We are trying to configure the DM816x USB0 as a serial device to configure the cell modem which we connected.

We are able to configure the USB in host mode and enabled CDC ACM modem driver as mentioned in the below document

http://processors.wiki.ti.com/index.php/Usbgeneralpage#USB_CDC-HOST

Booted the board with compiled uImage.

We are able to see the device in /proc/devices as "166 ttyACM".

But in /dev we didn't get any device created "/dev/ttyACM ".

We tried to create the device with the following command "mknod /dev/ttyACM0 c 166 0" and tried to open the device using "microcom". we get the following error

# microcom -s 9600 -X /dev/ttyACM0
microcom: can't open '/dev/ttyACM0': No such device

Can anyone tell me what mistake are we doing?


Thanks,

Srikanth.